9/23/2020 1:01 PM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello sam2014, if you have only one PC-Station for engineering and operating then you have a Single Station. No matter how many ASs or Remote I/O Station you have in your Project. The big different between a Single Station and a Multiuser Project is that, if you have a single Station (only one PC) you don't have to insert any OS path in the properties of the OS, if the OS path is empty PCS 7 knows that you have a single station. The rest is always the same. Insert a new ET200M, add the functionality of the S7-300 project to the S7-400 CPU, compile the OS. With regards |
9/23/2020 3:31 PM | |
Joined: 7/30/2014 Last visit: 4/16/2024 Posts: 145 Rating: (1) |
Thanks for reply I have two stations one is my old station that I told you (server / engineer / operator) and another operator station (new). my problem that when I run the configuration of my new station (target system ------> configure) the station does not appear in the list of accessible computers and when I run the configuration I get an error message " unable to access target computer "as if it does not speak and also in simatic shell I find my new station on the left but the right side is empty no settings appear |
Follow us on