11/26/2013 8:46 PM | |
Posts: 5 Rating: (0) |
Hello everyone, i have read a pdf file from Siemens teaching about communcation between 2 CPU 315 2dp via Profibus. Then i created a simple project for that using these PLC. The CPU connect to the master PLC by PC adapter MPI I also followed the instruction written in that book. Then when i tried download the program and hardware configuration of master first, it's ok. But then i downloaded the program and hardware configuration for slave, it is also downloaded to the master PLC. and the BUSF led flashed. The slave PLC didn't receive the program The program is working good if i plug the PC adapter MPI to each of CPU and then download their programs. My question is that, is there any possible way to download program from computer the slave PLC when we are plugging the PC adapter to the Master PLC? and How to configure that ? I try to find accessible node in PROFIBUS but i can't find because i think the Computer is not in the Profibus subnet. I also attach that ebook and the link: D6 - PROFIBUS DP with Master CPU 315-2 DP / Slave CPU 315-2DPThank you so much for reading it Attachmentd06_cpu315_cpu315.pdf (267 Downloads) |
11/27/2013 8:28 AM | |
Joined: 3/20/2013 Last visit: 4/3/2024 Posts: 676 Rating: (44) |
Hey! |
Last edited by: Fafner at: 11/27/2013 8:42 AMBest Regards, |
|
11/28/2013 3:56 PM | |
Posts: 5 Rating: (0) |
Hello, I have just make a test in this way: First i download the program + hardware configuration to the master via MPI port ( the PC adapter is plugged into the MPI port). Then i continuously plugged the PC adapter to the MPI port of the slave PLC and download its program + hardware configuration. Then after that, i reseted the slave CPU and clear its memory. Then i followed your steps and plug the pc adapter cable to the MPI port of Master PLC. It showed the note : "Online: the connection to the target module cannot be established" From that i have a question, DO we have to do sth to assign the profibus address of the slave PLC before downloading.? I tried finding the accessible node via "PLC > Displays accessible nodes" or PLC>Profibus>Assign Profibus address", The first one only show the master ( directly). The second one showed the notice: "right now you have made no Profibus interface ..." |
2/24/2017 3:09 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
New question published by davoimail94 is split to a separate thread with the subject 313C connect to another 313C PLC with MPI. Best regards |
5/8/2017 4:23 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
New question published by Palanivel is split to a separate thread with the subject How to access SLAVE PLC using ETHERNET in H PLC?. Best regards |
Follow us on