11/30/2014 12:47 PM | |
Posts: 7 Rating: (1) |
Hi William, I should have done that from the start, sorry. Now I've included the hardware, io and tags from my program. Regards, Hans Sietsema |
11/30/2014 2:02 PM | |
Posts: 5225 Rating: (1187) |
Hans, Thank you for the image. This should assist anyone that offers help to you. I am a bit rusted with the S7-300.. but it all seems okay. Did you check that IW800 is actually giving you a value? Please look at this: [LINK] Does this help you? w |
11/30/2014 4:27 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (713) |
Hello, Maybe this helps? Where and when do you need peripheral addressing? Regards, Marcjan |
Last edited by: Marcjan at: 11/30/2014 4:55 PMProblem solved? |
|
This contribution was helpful to1 thankful Users |
Follow us on