(0)| 6/22/2016 9:24 AM | |
|
Posts: 33 Rating:
|
Hi, I also got similar problem and the third party programmer downloaded to the HMI without enabling the backtransfer check box while downloading.So,I only can make image backup and can be used on identical HMI.Is there any other way to migrate to other HMI without having project file or need to start from beginning.(Build new application software from scratch)? Thanks, Min
------------------------------------------------------------------------------------------ |
Last edited by: Dany Min at: 6/22/2016 9:24:55 AMLast edited by: Min_Moderator at: 6/23/2016 11:51:07 AMNew subject after splitting |
|
| 6/22/2016 9:31 AM | |
|
Joined: 4/24/2006 Last visit: 1/14/2026 Posts: 9105 Rating:
|
Hello Dany Min, Then you will have to start from scratch. Best regards, Wizard |
This contribution was helpful to
|
|
Follow us on