11/10/2016 11:37 AM | |
Joined: 4/28/2015 Last visit: 4/7/2024 Posts: 58 Rating:
|
Hi all It seems to be a joke that it's not possible to rotate a symbol in TIA Portal v13. I've tried to rotate the symbol out of the TIA, but it lost resolution and waste a lot of time. I can't believe yet. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 11/10/2016 6:42:01 PMNew subject after splitting |
|
This contribution was helpful to
1 thankful Users |
11/10/2016 3:05 PM | |
Posts: 439 Rating:
|
Hello Autogen, Well, it is not a joke. You are able to use the "Animations" that are available. There is also lots of graphical objects in the "Graphics" toolbox, use them at your advantage.
I use "Gimp" which is a image manipulation program and .tif are the best image extension I found yet. If you lost resolution, then you have done something wrong somewhere. The "Alpha channel" permits you to remove the background and make it invisible. Best regards, Hugo |
Last edited by: HugoD at: 11/10/2016 3:05:40 PMLast edited by: HugoD at: 11/10/2016 7:11:53 PM |
|
11/30/2016 9:16 AM | |
Posts: 648 Rating:
|
Dear AutoGen_991924, you can use TIA openess and the rotation tool of the HMI Toolbox. Look at this hyperlink - Chapter: Simplified Engineering: https://support.industry.siemens.com/cs/ww/en/view/106226404 To your other problem: It is not possible to change the default graphic editor (MS-Paint). You have to use a other graphic program to design your graphics if you don't want to use MS-Paint. With best regards rh1990 |
This contribution was helpful to
1 thankful Users |
2/8/2017 3:50 PM | |
Posts: 1 Rating:
|
Hello everyone If you are trying to rotate an object by 90 then yes, it is possible and easy! Regards |
8/18/2017 8:37 PM | |
Posts: 7 Rating:
|
How do you do it? |
Follow us on