1/26/2018 2:49 PM | |
Joined: 2/26/2013 Last visit: 6/12/2024 Posts: 48 Rating: (0) |
Hello, first I apologize for jumping in your thread but I have also a similar question. We would like to standardize a little moulding cells with robot, which is connected to moulding machine by euromap67 and a central plc. An idea is to have a central plc in this way: Moulding machine <-> robot <-> central machine (plc) <-> periphery1, periphery2,.... The central machine will have also a HMI device which will display all diagnostics. The side with moulding machine, robot and plc is defined, but I need an information regarding connection of central plc with periphery units (modules). Every periphery unit will have its own plc 1200 but no hmi, because they will be small units. So my idea is that central plc would be the master and periphery units slave. I will define the communication handshake, but what would be the best way to communicate with (profinet,...?).... because there should be an option to add/remove periphery unit later and I don't want to change again hardware configuration of central plc. Are there any communication options which dont affect hardware configuration? Thanks and br ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/29/2018 9:47:39 AMNew subject after splitting |
|
Follow us on