5/20/2019 10:57 AM | |
Joined: 10/11/2006 Last visit: 9/5/2024 Posts: 5902 Rating: (803)
|
Dear abertoldo94, The G120 drives do have a HW limit switch function. E.g. CU240B/E-2 in section 6.10: https://support.industry.siemens.com/cs/ww/en/view/109757230/101839462923 This operates without encoder, but with limit switch. |
With best regards, |
|
5/23/2019 5:06 PM | |
Joined: 7/17/2018 Last visit: 8/1/2024 Posts: 16 Rating: (0) |
Hello, i have tried again but the situation is alway the same... I use the profidrive telegram 352 and the P1113 is high when i push the down button. But if i push the upper limit switch i can't muve my lift in down direction though i activate the P1113 and triggered P3340.
The drive remain in OFF3 AttachmentScreen.zip (258 Downloads) |
Follow us on