7/17/2012 8:11 PM | |
Joined: 11/2/2008 Last visit: 10/7/2024 Posts: 92 Rating: (1) |
Dear All, I am also facing the similar problem with my laptop i.e. when I am clicking on properties button of PC adapter Auto/MPI/Profibus/PPI I am getting following message "Your PG/PC has no local connection foroperating the device 'PC adapter'" I am getting option "none" in connection to paramterof local connection tab. Is there any solution for this? Thanks and regards |
Last edited by: O_Moderator at: 7/19/2012 10:12 AMnew subject after splitting from /tf/WW/en/Posts/57995#top |
|
7/20/2012 9:13 AM | |
Joined: 10/10/2005 Last visit: 10/18/2024 Posts: 1921 Rating: (136) |
Hello, I think the driver of USB adapter is missing and you have to install first or again in the PG/PC interface. I'm not sure but I can choise between COM 1, COM 3 and COM 4. But I have installed STEP 7 V5.5+SP2. See also the informations of the FAQ: http://support.automation.siemens.com/WW/view/de/37855422 With best regards |
6/24/2015 3:52 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
|
9/23/2015 2:40 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
New question published by Johnluck is split to a separate thread with the subject Cannot established connection with PC Adapter. Best regards |
Follow us on