1/4/2017 3:13 PM | |
Joined: 12/18/2014 Last visit: 9/22/2024 Posts: 33817 Rating: (4201)
|
At a maximum tank height of 2.30 m, a further 0.25 m has to be deducted because the minimum distance from the sensor to the medium is 0.25 m. In attachment the version adapted to your requirements. AttachmentFill_level_V3.zip (236 Downloads) |
This contribution was helpful to1 thankful Users |
1/4/2017 4:28 PM | |
Posts: 200 Rating: (6) |
Hi Thanks for the quick reply. i have added my program i cant seem to get the new settings right wounder if you could glance over it thanks Attachmentfill sensor.zip (267 Downloads) |
1/4/2017 4:48 PM | |
Joined: 12/18/2014 Last visit: 9/22/2024 Posts: 33817 Rating: (4201)
|
In B034 you use the wrong operator1. Do not add, but multiply. |
1/4/2017 5:16 PM | |
Posts: 200 Rating: (6) |
i changed this setting well spotted but when i transfer to my logo it does not seem to work correctly as it does in the simulation |
1/4/2017 5:44 PM | |
Joined: 12/18/2014 Last visit: 9/22/2024 Posts: 33817 Rating: (4201)
|
Since you do not write exactly what is in the LOGO! not working, I can only guess. Since I have no FS04, I can only check the program with my 0BA8.Standard. I have now made the necessary changes in your program. This included adjusting the bar graph in message text B031. In my LOGO! It works as desired. AttachmentPUMP V3 FB AI.zip (210 Downloads) |
1/4/2017 6:24 PM | |
Posts: 200 Rating: (6) |
hi i have converted to the standard logo AttachmentPUMP V3 FB AI (1).zip (249 Downloads) |
1/4/2017 6:42 PM | |
Joined: 12/18/2014 Last visit: 9/22/2024 Posts: 33817 Rating: (4201)
|
The file V4 evaluates the signal from the sensor as a distance and converts it to filling level. Try it with this version. AttachmentPUMP V3 FB AI_V4.zip (231 Downloads) |
Follow us on