1/4/2017 7:36 PM | |
Posts: 200 Rating: (6) |
when i use the version 4 one it works that when i get closer to the sensor as in tank filling up the numbers and graph go down in numbers rather than in up |
1/4/2017 9:17 PM | |
Posts: 200 Rating: (6) |
Hi I do apologize for the grammar i did not understand that you came from Germany. I have attached a copy of the version that works best. I have the sensor on the bench in the workshop. i have measured a distance from the sensor 2m300 to a object to simulate the bottom of the tank. From this measurement i have marked the following. low-Low Low High High-High For example i have the Low at 1320 and this is what it reads on the screen. What i dont understand is that if the tank is 2m300 why at this level does it not read for example 500mm off the bottom of the tank. hope this helps Attachmentv4.zip (301 Downloads) |
1/10/2017 9:31 PM | |
Posts: 200 Rating: (6) |
Alls gone well with the project few tweaks here and there but all good. Thanks |
This contribution was helpful to1 thankful Users |
1/10/2017 9:42 PM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33801 Rating: (4199)
|
That is very nice. I am glad for you that it works. |
Follow us on