Industry Online Support
Technical Forum
3/20/2011 8:38 AM | |
Posts: 81 Rating: (1) |
Dear All, Supose if we are using MTA in AO card and one module becomes faulty then other will take its place till here everything is Ok but can we reduce the switching time of redundancy because during switching MTA drops the output for 40ms or may be more can we reduce it to 20ms.
Splitted from AO in Redundant I/O. |
Last edited by: O_Moderator at: 3/21/2011 11:22 AMnew subject after splitting |
|
3/21/2011 11:23 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already published in the following thread redundancy of AO module through MTA for AO mudule. Best regards O_Moderator |
Follow us on