Industry Online Support
Technical Forum
12/17/2010 9:40 PM | |
Joined: 7/8/2009 Last visit: 12/7/2019 Posts: 1972 Rating:
|
There are Several ways to do this... Most people (I Prefer too) use Fixed Frequency Check out following /tf/WW/en/Posts/23634 Another way is to change over Data Set Check following http://support.automation.siemens.com/WW/view/en/7379354 Ofcourse these examples are for MM440 but it is also Applicable for MM420. Only change will be No of Frequency stepswill be limited asMM420having lesser No of Input compare to MM440 Regards, Devesh |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on