1/20/2009 4:14 PM | |
Joined: 5/28/2008 Last visit: 12/8/2015 Posts: 901 Rating: (136) |
|
Last edited by: *Manfred* at: 1/21/2009 11:15 AM |
|
1/21/2009 11:53 AM | |
Joined: 4/5/2006 Last visit: 9/16/2024 Posts: 917 Rating: (63) |
Hi Nitin, understood better now, i think this is already posted in ather thread... /tf/WW/en/Posts/25690#top and I think is not possible change connection as you want without stop RunTime Hope this link is what you are looking for Regards |
1/21/2009 12:07 PM | |
Joined: 4/5/2006 Last visit: 9/16/2024 Posts: 917 Rating: (63) |
Hello again, i seen you posted exactly same question i gave you in link well, you cannot change the network parameter like address by script, so have to look for different solution. Maybe you look this one http://support.automation.siemens.com/WW/view/en/2987284 configure in WinCC connection for both PLC (with different address), then uses the indirect address to point on tags for different boiler (same tag with different prefix/suffix). But you need change object properties to use indirect connection Then you can use import/export tool to duplicate tags for 2nd boiler Not exactly what you wanted maybe, but should be works Regards |
Follow us on