Industry Online Support
Technical Forum
5/23/2010 12:50 PM | |
Posts: 7 Rating: (0) |
Hi Mark Im working with a redudtant PAS server using IEC 61850 andIEC 101 slave and modbus master(version5.11)and my system has a redundant PASCC HMI too. i dont have any problem with both servers and all of the drivers are working properly. but i have a strange problem with PASCC! When my system is set to 2 servers and one HMI ( suppose it HMI1), its working without any problem even in redundancy and swichting between servers. but when im going to make the other HMI ( duplicated one) the problem is HMI2 is not working with both of the PAS servers. actualy it will work with the server that made the wizard for HMI2. the interesting thing is i've made the wizard file of HMI1with both of servers and tested it. it will work with wichever of them and in redudancy i don have any problem for swiching between servers for HMI1. but when i make the wizard file for example from server1,wizardrans and all the tags will be imported with201 exeptions(actually i have 201 errors in in message importing and i dont know wht!!). and my HMI2 will work with server1. till now its all ok . but when i want to switch between servers ( for example with shutting down the master server i.e. server1) hmi1will see this change and will change the server address i.e. server2( its icon in operation software will be green in a minute) but HMI2 ( that has the imported tags from wizard file of server1)will have the compkey and project ID error and will be shut down the pasCC. the worth thing isthe compkey of hmi2 is the same as setting of serverand rather than this, the compkey of both servers for hmi2 are the same(32) and are equal to the compkey of hmi2. and the project iID in both servers are1. I dont know what is wrong with this system. I should say that when i am trying to run hmi1 project on hmi2 PC (for testing harwares and softwares of hmi2 of course with changing the name and IP of PC2 similar to PC1 and shutting down the PC1 of HMI) there is no problem at all and the project works. but when im going to use the PC2 as hmi2 (Dupplicated)with wizard of server1, when server2 is master, it will have this error. If anyone could help me it will be appreciated. Soroush Splitted from If anyone needs information/manual/catalogs about Sicam PAS, SAS, RTU, eRTU and Siproted/Digsi, please let me know. |
Last edited by: O_Moderator at: 5/25/2010 8:46 AMnew subject after splitting |
|
5/25/2010 8:48 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already published in the following thread Compkey and Project ID error Between PAS and PASCC. Best regards O_Moderator |
Follow us on