4/29/2012 9:28 AM | |
Joined: 12/1/2009 Last visit: 3/31/2024 Posts: 672 Rating: (147) |
Very strange Saravana kumar , It could be that you have a problem with one AS, but as per my experience I doubt. I would say that your block has a generally problem and you are just "lucky" that it works in all other AS as per your expectation. Check your block for temporary variables you read but not write in this block. Regards. |
Give us your feedback and show us your respect! |
|
This contribution was helpful to1 thankful Users |
4/30/2012 12:40 PM | |
Joined: 11/4/2011 Last visit: 12/8/2023 Posts: 253 Rating: (53) |
Hi, I meant that I would open that FB and look at how the signals are processed.
So I'd go from the output bit 6 up to the inputs that are affected in the forming of the wrong output signals. It is possible to specify the FB's instance when you open FB and go online: How can you monitor a block with the desired call environment in STEP 7? |
4/30/2012 1:48 PM | |
Joined: 12/1/2009 Last visit: 3/31/2024 Posts: 672 Rating: (147) |
Dear Saravana kumar, SCL is my favorite, esspecially when it is getting used for simple logics. Anyway, you need to install SCL editor to check the logic of your block. Regards. |
Give us your feedback and show us your respect! |
|
5/1/2012 12:05 AM | |
Joined: 11/4/2011 Last visit: 12/8/2023 Posts: 253 Rating: (53) |
Saravana kumar, ES is without SCL Editor, but is SCL Source file still present in the project library? If yes, you can open it in Notepad then. So open Project_Lib\s7asrcom\00000001\ folder and look up in *.SCL files for your FB's source. At least you can see a logic of FB in handy representation. And after all someone can recompile fixed source for you just for free (even me). And what about PLC Simulator? Yet another way to test your FB performance. Oh, and I've just thought of some possible reason of your troubles: your problematic FB is using another FBs/FCs which differs in old and new AS. Is it possible in your case? And 2Experts: is it possible at all? Regards. |
Follow us on