3/30/2010 6:12 PM | |
Joined: 3/30/2010 Last visit: 7/26/2021 Posts: 13 Rating: (0) |
CPU 315-2PN-DP (Master) & CP 342-5DP(slave) communication 1. I want to connect CP342-5dp present in another PLC panel to My PLC 315 2pn-dp through profibus. 2. I have configure CPU-315 DP port as a master. And connect 1 profibus link on DP port. 3. On Same link I have connect the CP342-5dp as a slave. 4. This configuration is downloaded but error come on plc .SF & bf-1 led is glow.I check the mlfb no. both end are same. The customer cp parameter is as belowCommunication processor cp342-5dp DP address:12 Mode of operation: dp slave passive Third party send the 72 byte data & receive the 14 byte data.( AS per addr. Listprovided by Customer)
Attachmentref.zip (65 Downloads) |
Last edited by: O_Moderator at: 3/31/2010 10:13 AMnew subject after splitting from /tf/WW/en/Posts/1174#top |
|
3/31/2010 10:47 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already published in the following thread Conect CP 342-5dp as a slave to Mster CPU -325 2pn-dp. Best regards O_Moderator |
Follow us on