12/2/2015 6:42 AM | |
Posts: 16 Rating: (0) |
Hello, I have a S7 200 CPU224 which is flashing SF/DIAG and STOP lights. I installed Microwin & SP9 V 4.0.9.25 into win 7 I use the USB - PPI RS485 ( 2013) cable. The cable shows as installed in WIN Device Manager and GREEN TX lights flash when I try to communicate with PLC No RED RX lights. Microwin reports error Communication timed out check port number, network address, baud rate and attached cable. I have tried using the settings as per the manuals (2011) but cannot communicate with the PLC. Help please. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/2/2015 1:26:09 PMNew subject after splitting |
|
2/14/2016 8:40 AM | |
Posts: 16 Rating: (0) |
Sorry attachment not clear. |
2/14/2016 8:12 PM | |
Posts: 5225 Rating: (1192)
|
I have lost track of this post.
When making connection it is recommended: w |
2/15/2016 8:34 AM | |
Posts: 5225 Rating: (1192)
|
Duris - I have never used Profibus connection to link to an S7-1200.. for me it is always PPI. Even the multi protocol adapter is using PPI. I cannot even remember having to set USB on the PC Adapter settings. Also.. I have multiple types of PPI cables dating even from ca. 1996 :: serial / usb / PC adapter. All cables work with computers installed with Windows 7 (Prof) - but with the patch as linked to in my earlier reply. What I do know is that I had one PC adapter that did not link to S7-200 anymore but worked in MPI on S7-300. I replaced the PC adapter without changing any drivers and it worked again perfectly. Duris - I am very thankful for your help in this topic.. but I think it is best that this topic be handed over to the Siemens Support guys to formally sort out this issue. <bremaster22> please contact the Siemens guys on |
This contribution was helpful to1 thankful Users |
2/15/2016 9:30 AM | |
Posts: 16 Rating: (0) |
This is the adapter, all 3 lights are steady green. the MPI light blinks when I try different comunication combinations. |
Follow us on