7/8/2020 1:50 PM | |
Joined: 8/3/2009 Last visit: 5/14/2024 Posts: 12944 Rating: (1648)
|
Hello If you work with PLC alarms, or Diagnostic view or other Tmestampls out of the PLC or you have a NTP Serve rin the System then you should not use the Area Pointer for time Synchronisation because you will not get a suitable result. Just use Time syncronisation methods which are based on UTC. here are the two FAQs that tells you averything you need:
Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on