6/23/2016 2:11 PM | |
Posts: 171 Rating: (43) |
Am also getting the same problem " Input/output data not available" Even I removed the DI and DO's. Connected the server module itself... Existing version of server module is V1.1.1. But am having only V1.0 in my TIA V13 SP1 UPD7. Also installed the available HSP's till now. Help me getting the latest HSP or solve this.
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/24/2016 1:33:11 PMNew subject after splitting |
|
This contribution was helpful to1 thankful Users |
6/23/2016 3:18 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, Latest Upd 8 Updates for STEP 7 V13 SP1 and WinCC V13 SP1 - Siemens Industry ... Support Packages for the hardware catalog in the TIA Portal (HSP) - ID ... |
Last edited by: Ste39 at: 6/23/2016 3:27:19 PM |
|
6/23/2016 8:09 PM | |
Joined: 8/14/2015 Last visit: 4/30/2022 Posts: 12 Rating: (0) |
Hi, Do you have an answer yet? I have the same problem. Thanks, |
6/24/2016 1:34 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4775 Rating: (123) |
New question published by EAriasCarr is split to a separate thread with the subject ET200SP NO SERVER MODULE IS CONFIGUREDF. Best regards |
6/25/2016 8:00 PM | |
Posts: 171 Rating: (43) |
Don't know how, bt finaly i solved it... Just downloaded it with version V3.1 to ET200SP,,, thn all shows green... |
7/7/2016 5:33 PM | |
Joined: 1/18/2014 Last visit: 4/2/2024 Posts: 4 Rating: (0) |
I have the same problem, TIA Portal V13 SP1 update 9 offers me only 6ES7193-6PA00-0AA0 V1.0. Does anyone have a solution? |
Follow us on