4/20/2012 1:10 PM | |
Joined: 4/24/2006 Last visit: 9/19/2024 Posts: 8739 Rating: (1168) |
Hello avafab, Have a look at the following links: how do you specify the runtime of a timer by means of an operator panel and how do you output the remaining runtime? how can you convert a number value of the data type INT into a string in S5TIME, or into the data types BCD and REAL? Best regards, Wizard |
This contribution was helpful to1 thankful Users |
4/20/2012 1:14 PM | |
Joined: 4/20/2007 Last visit: 9/19/2024 Posts: 725 Rating: (42) |
Look at my last post in this topic. That is what I use :-) |
4/20/2012 1:31 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Hello, Check this straight forward and concise solution: L MW 10 // in sec ITD L 1000 *D T #zhd1 CALL "TIM_S5TI" IN :=#zhd1 RET_VAL:=MW12 Best regards, Hamid Hosseini Attachmentint2s5time.zip (637 Downloads) |
Last edited by: hdhosseini at: 4/20/2012 2:03 PM//S7 project uploaded |
|
This contribution was helpful to1 thankful Users |
4/24/2012 2:39 PM | |
Posts: 83 Rating: (1) |
Which function I can use to do the same in ladder? thank you can I use this into FB?
|
4/24/2012 3:08 PM | |
Joined: 4/20/2007 Last visit: 9/19/2024 Posts: 725 Rating: (42) |
Hi, Please find attached the FC I always use... Hope you will find good use for it. AttachmentInt_to_t.zip (686 Downloads) |
Follow us on