6/12/2013 7:56 PM | |
Posts: 4 Rating: (0) |
Hello Everyone, I have a hardware downloadproblem with Simatic Manager. In the hardware I have many I/O modules and also two Simotion CPUs. One of them is Simotion D445 and the other is Simotion D425. I upload the program by opening a blank project and selecting Upload Station to PG from the CPU 424-2DP and then I press on the download button without no change but it gives an error "The slave C2xx/P3xx/D4xx ISlave in the DP master system Profibus DP Machine: DP master system (1) does not contain an assignment of the logical master/slave addresses." If I remove the station boxes of these two simotion CPU the error does not occur. You can see the screenshots from the attachemets. What can I do to solve this issue? What is the problem. The configuration inside the CPU is not correct? How can I add an assignment of logical master/slave addresses? AttachmentHardware.zip (172 Downloads) |
6/14/2013 4:19 PM | |
Joined: 10/11/2006 Last visit: 4/26/2024 Posts: 5825 Rating: (789)
|
Hello, If its an engineering problem it would be necessary to contact the hotline: Tel: +49 (0) 911 895 7222 Fax: +49 (0) 911 895 7223 Online Support : http://www.siemens.com/automation/service&support Support Request : http://www.siemens.com/automation/support-request |
With best regards, |
|
6/16/2013 7:07 PM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
Hello, why a new thread? is the same problem you described here /tf/WW/en/Posts/92959#top |
6/17/2013 9:47 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
check the answer in the other thread ! |
6/17/2013 9:56 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Hello together, i now closed the other thread, and copied the answer from ChristophD to this thread here. Please note that it is not good to publish questions in forum twice. Best regards O_Moderator |
This contribution was helpful to1 thankful Users |
Follow us on