6/9/2011 10:55 AM | |
Posts: 89 Rating: (7)
|
Hello, you said you got an bundle of the microbox. So you got the WinAC RTX installed. With this SoftPLC it is possible to do open user communication (OUC). OUC means TCP/IP, ISO on TCP and UDP comm. Have a look to these FAQs to have a better start: http://support.automation.siemens.com/WW/view/en/25209116 http://support.automation.siemens.com/WW/view/en/29737976 regrads, Moldi |
6/9/2011 11:32 PM | |
Posts: 3093 Rating: (323) |
Hello Aurel18, do you want to use ModbusTCP for communication? If yes, take a look here. The Modbus package for PN-CPUs runs with WinAC as well. Regards, Kaulquappe |
6/10/2011 2:58 PM | |
Joined: 1/26/2011 Last visit: 8/11/2022 Posts: 243 Rating: (67) |
For ModbusTCP communication you can try to use this Wizard. http://support.automation.siemens.com/WW/view/de/31535566 |
6/10/2011 9:37 PM | |
Posts: 3093 Rating: (323) |
But the wizard won't help without the Modbus block. Regards, Kaulquappe |
6/14/2011 9:39 PM |
|
Posts: 947 Rating: (45) |
Hi Kaulquappe What I wrote about the UDP can be applied to TCP (The same wizard, same FAQ, the same chapter in the manual of SFC ) |
6/14/2011 10:19 PM | |
Posts: 3093 Rating: (323) |
Hi gre_m, but the question was to connect a Microbox and a PAC. Regards, Kaulquappe |
6/17/2011 10:20 AM | |
Posts: 947 Rating: (45) |
Hello Kaulquappe Pac3200 has interface RS485, Profibus and some models ethernet. For Connectby ethernet you can gateway (rs485, profibus) to ethernet. if your model has internal ethernet port? then you can direct connect. PAC3200 use variety TCP - Modbus TCP. You can buy addons from IT4Industry or write own programm. For this need FB for open communication and wizard (That's what I wrote above). Usefull FAQ on customer support http://support.automation.siemens.com/WW/view/en/32048373. No complications in the no. Open communication in WinAC RTX used internal Ports (IF1..IF4) - where in Microbox instaled Profinet card |
Last edited by: gre_m at: 6/17/2011 10:28 AM |
|
Follow us on