3/21/2017 9:25 AM | |
Joined: 2/20/2014 Last visit: 4/25/2024 Posts: 395 Rating: (38) |
Hi, I have connected one Ethernet cable from IOT 2040 to my laptop & another Ethernet cable from IOT 2040 to the wifi router but when i try to ping using "ping www.google.com", i only get the following: "ping: bad address 'www.google.com'". Can anyone here advise me on how i can make a successful internet connection to the IOT 2040? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/21/2017 3:07:43 PMNew subject after splitting |
|
3/21/2017 9:40 AM | |
Posts: 71 Rating: (16) |
Is DHCP enabled for the port you use to connect to the router? Use iot2000setup to check and/or reconfigure. |
This contribution was helpful to1 thankful Users |
3/22/2017 8:46 AM | |
Posts: 531 Rating: (34) |
dns 8.8.8.8 as DNS Server to the ip setting does not help? |
This contribution was helpful to1 thankful Users |
3/22/2017 10:11 AM | |
Joined: 2/20/2014 Last visit: 4/25/2024 Posts: 395 Rating: (38) |
tried already, same as earlier unable to ping www.google.com |
3/22/2017 11:01 AM | |
Posts: 531 Rating: (34) |
What happens if you use the ip itself. Ping on another pc and use that google ip adress to check whether dns resolving is the problem or something else. |
3/22/2017 11:02 AM | |
Posts: 531 Rating: (34) |
If it is dns related, you can try to ping on pc and take the ip address and ping with that instead of google.com on the IoT 2040. |
3/23/2017 1:30 AM | |
Joined: 2/20/2014 Last visit: 4/25/2024 Posts: 395 Rating: (38) |
Yes i can ping my engineering PC with my IOT
|
3/24/2017 1:49 AM | |
Joined: 2/20/2014 Last visit: 4/25/2024 Posts: 395 Rating: (38) |
Yes i can ping the router as well.
|
3/28/2017 8:01 AM | |
Posts: 215 Rating: (6) |
It should work with "db1,x0.0" instead of "db1,Bool0". |
This contribution was helpful to1 thankful Users |
3/30/2017 8:18 AM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
Hi karthikk, for this purpose you can use the Siemens IOT2000 Input/Output module. With this shield you have the possibility to send TWO digital outputs (24V) from your IOT to the S7-1200 CPU. If you want to have more outputs or outputs which are not boolean you can use i.e Modbus TCP to communicate. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
Follow us on