6/17/2010 9:02 AM | |
Joined: 9/18/2006 Last visit: 5/3/2024 Posts: 589 Rating: (64) |
Hi. You try to make so: 1) To change 38000 2) To create NC-archive 3) To load this NC-archive. Best regards. |
6/17/2010 10:21 AM | |
Posts: 2964 Rating: (479) |
Hi... Anyentry in Axis MD parameter38000 will cause "Memory Re-organization". So what you should means in that condition take a NC archive bacup and give an NCK reset, then reload the NC archive backup which was taken in memory reorganized condition. Now you should able to see your compensation data. I have write up for LEADSCREW PITCH ERROR COMPENSATION you can check the same. Hope this infromation will be useful to you..... Ekalavya AttachmentLPEC.pdf (887 Downloads) |
This contribution was helpful to4 thankful Users |
6/19/2010 7:53 AM | |
Posts: 159 Rating: (1) |
Machine is now compensated!!!! Thanks for the help guys!!! Craig. |
Follow us on