10/31/2014 2:48 PM | |
Joined: 11/23/2011 Last visit: 9/17/2024 Posts: 202 Rating: (32)
|
Hello martycochrane, I can answer your question about the "standard way" to connect in relation to LOGO! 8. An easy way for simple switching like a light is to use the integrated webserver of LOGO! 8. Here you have an example of the manual how the webserver works an how it is designed: Operating webserver LOGO! 8 connection works with Ethernet. In the past at older LOGO! modules there was also the possibility to connect witha LOGO!-PC cable to the RS232 interface of the PC. But now Ethernet is the standard. For other PLCs maybe you have to ask in the specific conferences. Do you know which kinds of Siemens PLCs are available? Hope this information is quite helpful for you. Have a nice weekend. Greetings, KM_AS |
10/31/2014 3:33 PM | |
Joined: 11/23/2011 Last visit: 9/17/2024 Posts: 202 Rating: (32)
|
Hello martycochrane, you don`t need a server to handle the communication of LOGO! and HMI. You can connect directly to the HMI with Ethernet. Here you have an FAQ and some examples for LOGO!-HMI connection. The application examples describe an house control with LOGO!-HMI,also with switchinglights on/off among other thinks. FAQ: How do you establish a connection between a LOGO! 0BA7 and an HMI Panel? Application examples LOGO!-HMI: http://support.automation.siemens.com/WW/view/en/68585344 http://support.automation.siemens.com/WW/view/en/68585346 When you need information about LOGO! and OPC-server there are already some topics about this in the forum, f.e. this topics: NI OPC Servers LOGO! 0ba7 OPC Server for LOGO! OBA7 Logo! 0BA7 and Simatic Net Hope the information is helpful for you. Greetings, KM_AS |
4/7/2015 1:12 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|
4/15/2016 10:05 PM | |
Joined: 4/30/2011 Last visit: 1/9/2022 Posts: 223 Rating: (4) |
Any news? Is there a possibility to use LOGO! 8 HTTP Api ?
|
This contribution was helpful to1 thankful Users |
11/27/2016 2:21 AM | |
Posts: 2 Rating: (0) |
Hello, I know that this post is quite old but why do you say that an http api is not possible? Regards, Lucas |
Follow us on