9/21/2010 12:18 PM | |
Posts: 20 Rating: (0) |
Hi , I have a ES and aseparate OS/CLIENT. i am upgrading and adding another client machine. When i downoad to the client it gives me a message "error occured during download to target system" the project is on the client machine but when i try to open it it says access to the project is currently not allowed. what could be causing this?
Splitted from Client error. |
Last edited by: O_Moderator at: 9/21/2010 2:04 PMnew subject after splitting |
|
9/28/2010 7:38 AM | |
Posts: 325 Rating: (13) |
Hi Jeph, Change the Client OS name in the Engg Station and make surethat OS name should be same as that of Engg station name. During download the Client OS name will get automaticallty changed to that of the Client's machine name. I hope u have given enough permissions on the Client's Folder where u want to store the client project. Also just make sure that u have logged in to Clients machine as an Administrator. Rgds Nil Check this link ..... /tf/WW/en/Posts/39406 |
10/1/2010 1:46 PM | |
Posts: 20 Rating: (0) |
the solution in the end was that i had to unistall the network card then re-install it. thanks for your help
|
This contribution was helpful to1 thankful Users |
4/23/2012 2:08 PM | |
Posts: 133 Rating: (9) |
Hi Jeph I have a feeling that when you re-installed your network adaptor. It resolved the conflict in the Configuration console. I have created a document on how to resolve this problem in some detail. I know that your problem is solved but maybe if you are interested you can download it on the following link. I took a few screenshots in the document. /tf/WW/en/Posts/72897#top Regards Bilal Moolla |