7/8/2013 6:58 PM | |
Joined: 8/27/2006 Last visit: 4/23/2024 Posts: 719 Rating: (88) |
YES. It takes a complete image of the first panel and copies it to the second panel, like when you make a ghost image of your PC.
|
The more you know, The more you know that you don't know |
|
7/8/2013 7:34 PM | |
Joined: 5/28/2008 Last visit: 5/11/2024 Posts: 4506 Rating: (836) |
Hello,
Hope this helps. |
Ayman Elotaify |
|
7/8/2013 8:20 PM | |
Posts: 559 Rating: (87) |
Try with pc/ppi multi master cable with boot reset. |
This contribution was helpful to1 thankful Users |
7/9/2013 6:50 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Dear Ayman Elotaify I have already tried the Prosave + reset to factory settings as per the FAQ. I have the same problem with this. Cheers Navnag |
There is no such thing as the last bug in a program |
|
7/9/2013 7:15 AM | |
Joined: 8/27/2006 Last visit: 4/23/2024 Posts: 719 Rating: (88) |
Dear Navnag, try the USB flash and it will do the job. If you can't connect to the second MP, then maybe something wrong with the configuration on the MP itself or the OS is corrupted. When you copy from the first MP to the second one, all the settings will be reset as the first screen. You need a USB flash not smaller than 2GB.
|
The more you know, The more you know that you don't know |
|
This contribution was helpful to1 thankful Users |
7/9/2013 7:32 AM | |
Joined: 4/17/2012 Last visit: 3/30/2024 Posts: 474 Rating: (10) |
Hi, After factory reset just check the communcation setting options and If you have ethernet option check the Pinging information. |
7/9/2013 8:31 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Dear DS SURESH KUMAR I have already mentioned in my previous post that we are not able to even give factory reset !! So we cannot reach the stage of changing the parameters "After Factory Reset" The HMI is visible in "View Accessible Nodes" on Profibus as well as "Pinging" in Ethernet. Dear AMAZINGAHMED I am back from the site. Presently we loaded the software on a spare HMI available with the customer. Will definitely try your suggestion and post the results here. Thanks Navnag |
Last edited by: Navnag at: 7/9/2013 8:35 AMThere is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
7/9/2013 8:33 AM | |
Joined: 5/28/2008 Last visit: 5/11/2024 Posts: 4506 Rating: (836) |
Hello, If you already tried all above sugessions, and if you are completely sure that the setting of the MP is typically like the first one, then contact your local Siemens office. Please see puti's reply of thisthread. He found that he bought some panels without image or without a complete image. So may be something wrong with your panel itself. And if you are still within warrenty, Siemens will replace this panel for you. Hope this helps.
|
Ayman Elotaify |
|
7/9/2013 8:36 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Hello, yes i agree with Ayman. Problem looks in MP. Go for Support Request |
VANDE MATARAM..... |
|
7/9/2013 8:37 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Dear Ayman Elotaify Thanks for the suggestion. I too feel the Panel OS is currupted. Unfortunately the units are not in warranty. These have been working fine for last 4 years. We were now trying to add some new Alarms in the HMI panels when we encountered this problem. Thanks Navnag |
There is no such thing as the last bug in a program |
|
Follow us on