Industry Online Support
Technical Forum
12/1/2014 4:20 PM | |
Joined: 12/1/2014 Last visit: 2/2/2024 Posts: 5 Rating: (0) |
Hi, I have the same problem (I think so...). I have installed Tia Portal V13 update 6 in Windows 7 Ultimate 32Bits. I'm using PC Adapter v5.1 (6ES7 972-0CA23-0XA0). In online accesses I can't see any PC Adapter. Although, if I enter in "Set PC/PG Interface" through Control Panel, I can select PC Adapter (Auto, MPI, DP). If I select PC Adapter (Auto), I can autodetect network parameters (profile, speed, etc). It shows me that driver is Ok and the problem is in Tia Portal, it isn't? Thank you for your support. EDIT: If I connect the PC Adapter RS232, It appears in TIA Portal like COM3. But I can't use it to find devices.
------------- new subject after Splitting from PC adapter MPI for TIA Portal V12 |
Last edited by: CS Moderator at: 12/2/2014 10:44 AMsplitting Last edited by: jgutierrez at: 12/1/2014 5:27 PM |
|
12/2/2014 10:45 AM | |
Joined: 9/1/2005 Last visit: 9/18/2024 Posts: 4104 Rating: (195) |
closed cause question published more than once. The second thread with the subject TIA PORTAL v13 - PC Adapter v5.1is published within the same conference. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on