9/14/2012 9:49 AM | |
Posts: 20 Rating: (0) |
Thanks for the response will try this. |
9/2/2015 10:22 AM | |
Joined: 3/19/2015 Last visit: 4/8/2024 Posts: 22 Rating: (0) |
Hi does it need to download HWconfig to PLC or just a calution is used for compiling the Code?
|
9/2/2015 10:52 AM | |
Joined: 1/28/2009 Last visit: 4/26/2024 Posts: 6838 Rating: (1359) |
Hello ,
You enter the actual work memory required for DBs in Calculate monitoring time and press "Recalculate". If the new values differs from the old calculated time (it may happen in big changes) , it is possible to download the new values"Monitoring Times" even your system is in RUN.Check the manual for fault tolerant CPUs for more information. I hope this helps, hdhosseini Attachmentpara.rar (266 Downloads) |
This contribution was helpful to1 thankful Users |
9/3/2015 2:34 AM | |
Joined: 3/19/2015 Last visit: 4/8/2024 Posts: 22 Rating: (0) |
thank you for replying. i have change memory from 1024kb to 5048kb, which came in download warning and the result is as attachment. does it will affect any thing in the CPU performances or only memory allocation? AttachmentMemory chage.zip (337 Downloads) |
11/8/2016 9:40 AM | |
Joined: 8/21/2014 Last visit: 4/26/2024 Posts: 951 Rating: (13) |
New question published by Ali00 is split to a separate thread with the subject Limit on Max. Scan cycle time extension?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on