(3)| 5/29/2018 11:25 AM | |
|
Joined: 3/13/2018 Last visit: 11/1/2024 Posts: 1 Rating:
|
Hi all, I have also installed Protool SP3 but this time in Windows 10. I used an Protool installation CD and select the compatibility mode <Window XP (sevice pack 2)> The installation work without major problems needed to select ones the OK button. After installing the program I also selected the compatibility mode <Window XP (sevice pack 2)> for the protool.exe to start the program. I cannot start up direct from the step 7 project the protool project I need to go the panel sub folder with the protool project data. I also test to download the software into OP17 panel and this also work without any problem. I needed to change my USB-Serial adapter to COM1. But the rest I could download the project ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 5/29/2018 2:23:52 PMNew subject after splitting |
|
This contribution was helpful to
|
|
| 6/25/2021 9:14 PM | |
|
Joined: 7/10/2015 Last visit: 12/30/2024 Posts: 1 Rating:
|
solved steps as attached photos |
This contribution was helpful to
|
|
| 7/28/2021 9:06 AM | |
|
Joined: 5/28/2008 Last visit: 10/29/2025 Posts: 4522 Rating:
|
Hello, From picture No. 5 shared in the previous post, go to file and click on integrate with Step 7 project. |
|
Ayman Elotaify |
|
| 9/20/2024 1:02 PM | |
|
Joined: 3/6/2014 Last visit: 10/18/2025 Posts: 3 Rating:
|
That's not the final solution... |
Follow us on