5/17/2017 11:41 AM | |
Posts: 27 Rating: (0) |
dear sir if u have command address manual of g120 ( cu240e-2). pls send me thanks |
5/17/2017 11:50 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
Hi, install Startdrive to add the G120 to the HWCatalog of tia. Then create a S7-1200 and from the catalog select the G120 you need. Now you can configure a data transfer telegram on the G120 in Device properties . You can create a speedaxis on the S7-1200 and connect it woth the G120, now you can use the MotionControl commands in your block on S7-1200. What you mean with command adress manual? Application Example: https://support.industry.siemens.com/cs/ww/en/view/70155469 Regards Christoph |
5/17/2017 12:34 PM | |
Posts: 27 Rating: (0) |
|
5/17/2017 12:37 PM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
https://support.industry.siemens.com/cs/ww/de/view/109741912 |
5/17/2017 12:44 PM | |
Posts: 27 Rating: (0) |
dear sir this link is in german language, can u send me in english version thanks |
5/17/2017 12:49 PM | |
Posts: 27 Rating: (0) |
dear sir can u also send me hsp firmware v4.7 start up file for tiav13. thanks |
5/19/2017 6:22 AM | |
Posts: 27 Rating: (0) |
|
Follow us on