4/20/2012 2:16 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Dear All, is it possible to replace CP1413 Card with CP1613 Card? Thanks in Advance. |
VANDE MATARAM..... |
|
4/20/2012 2:46 PM | |
Joined: 7/18/2011 Last visit: 10/9/2023 Posts: 521 Rating: (90) |
Hi Amit_86 I think this thread contains the answers for your question. Kind regards, BV |
4/29/2012 6:25 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello everybody, Some previous responses made the confusion with the CP1430 that is a Simatic S5 card (successor of the CP535). The CP1413wasa PC Card thatwas fitted in an ISA slot of the PC Because ISA slotswere not available in new PCs, the CP1613 was introduced. See: http://support.automation.siemens.com/WW/view/en/4246763 The CP1613 is howeverfits only in aPCI slot. Conclusion: You cannot just pull the CP1413 and place a CP1613 in the same slot. |
Best regards |
|
This contribution was helpful to3 thankful Users |
4/29/2012 6:31 PM | |
Posts: 1064 Rating: (72) |
that is exactly my mistake thank you for the clarification |
This contribution was helpful to1 thankful Users |
4/30/2012 4:04 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
HelloJKLM, Thanks for all important link and information. Well, I know that CP1413was previously hooked up on ISA Slot and Because ISA slotswere not available in new PCs, the CP1613 was introduced. Now letus say i am replacing PC withCP1613 Card and on S5 side i am not changing anything thenis it work? My Clientis not intersted to change anything on S5 PLC Sidesince the Plant is running without any problem and they have enough spare for S5 PLC. But letus sayin futureif problem comesin running PC then it is diificult toarrnage such old PC with ISA Slot. I hope now everbody understood my requirement. Thnaks inAdvance. |
VANDE MATARAM..... |
|
Follow us on