4/14/2020 8:14 PM | |
Joined: 2/5/2013 Last visit: 5/2/2024 Posts: 320 Rating: (74) |
Hi Lupinlll, I hope you have original program with you.You can do one thing.Before changing web server related settings in program you can take snapshot of DB variables in original program and use that program to change web server related settings so that even after downloading modified hardware.It can not change DB parameters. This link will help you regarding snapshot. As you are changing web server related settings on S7-1200 controller then you have to compile hardware and download it in controller. Br, AmolG. |
Last edited by: AmolG at: 04/14/2020 20:30:06Last edited by: AmolG at: 04/14/2020 20:32:11Last edited by: AmolG at: 04/14/2020 20:37:40Please rate it. |
|