6/25/2007 3:09 AM | |
Posts: 2 Rating: (0) |
Hello All. Attachmentflum43.zip (233 Downloads) |
6/26/2007 2:55 AM | |
Posts: 191 Rating: (58) |
Hi!! try this.. check the changes in the datablock... you still have to re-type the messages but could work.. tell me if it works. Attachmentfl 2.zip (246 Downloads) |
7/2/2007 9:21 PM | |
Posts: 2 Rating: (0) |
Hello. Thanks for your answer. Your file is the best way to get a solution ... Today, i call Siemens support service, and the serviceman tell me the datas is shown in the hexadecimal... and need to convert to ASCII code. Then i compare with a other good program file .. to see how the file is ... (the strings ...40 characters,between "quote" ...begin and end charaters delimiter. And with function hextoascii, i convert the hexadecimal code .. to ascii code ... and is OK .... After building the entire data block, i compare with the plc ... and display not equal .... due to change of the format type of the new block built by me . After rechecking (traduct of strings .... and the location for the embedded values), i connect to the plc .. and i download only my data block .... I test the machine ... and the display and data edit values is OK ... After new plc comparison with my PC , now all is equal ... and all is OK ! Now , i can edit the strings to the TD200 .. no problem !!! I send the file .. corrected by me ..with the help of the Siemens serviceman. I send, if you are interested, the corrected project and a little program made by me with Borland Delphi 6, to convert hexadeciamal code to ascii code. Greetings from France. Stéphane. Attachmentflum_and_converter.zip (225 Downloads) |
Follow us on