6/27/2010 10:11 AM | |
Joined: 2/6/2009 Last visit: 3/21/2024 Posts: 938 Rating: (118) |
Dear All, Here I have attached a program backup contains the block for"Set/Reset Range" of bits.This block is like Set/Reset option in Step7 MicroWin. The block can be used for both Set as well as reset. This block is not having anydependencywith MCR. This can be used for Memory Bits, Digital Outputs and DB bits. Revert back for any clarification. AttachmentSet&Reset_Bits.zip (177 Downloads) |
Last edited by: Saravana kumar at: 6/27/2010 10:14 AM_______________________________________________________________ |
|
This contribution was helpful to3 thankful Users |
6/29/2010 5:54 PM | |
Joined: 2/6/2009 Last visit: 3/21/2024 Posts: 938 Rating: (118) |
DearY.DHINAKARAN, I am not able to get your question clearly. Can you ask in brief. The use of the block is to Set / Reset Range of Bits in Memory Bits, Digital Outputs or DB bits.
|
_______________________________________________________________ |
|
Follow us on