Industry Online Support
Technical Forum
6/20/2010 4:33 PM | |
Posts: 122 Rating: (1) |
Hi everyone, I wanted to simulate my Panel-PLC network and I did exactly what you said, Saravana. It works! I'm so happy! The only different thing is that I'm running it through PLCSIM(PROFIBUS). I don't know why but it's the only way I could do it. Does it have something to do with the network configured in NetPro?? Thanks for the help!! Sara Splitted from WinCC Flex 2008 and PLC SIM V5.4. |
Last edited by: O_Moderator at: 6/21/2010 10:41 AMnew subject after splitting |
|
6/21/2010 1:48 PM | |
Joined: 2/6/2009 Last visit: 8/19/2024 Posts: 939 Rating: (118) |
DearSaruca, There is no need to do any configuration setting in the netpro. I had not done any setting in netpro. Just I have created a project with integrated WinCC Flexible project. I thing now your doubt is cleared. Revert back for any clarification.
|
_______________________________________________________________ |
|
6/21/2010 1:51 PM | |
Posts: 122 Rating: (1) |
I understand. Both matters are not related. Thanks Saravana! Sara |
Follow us on