12/23/2009 4:11 AM | |
Posts: 153 Rating:
|
Hi,liew. First.You can use two LOGO!.For example: https:///tf/WW/en/Posts/38357#top The logic module is simple in programming and in operation. It allows to introduce and use quickly it in different systems. Second.To use such products as S7-1200 or S7-200. |
12/23/2009 3:10 PM | |
Posts: 173 Rating:
|
With 2 LOGO!'s (both with full I/O expansion modules) and with 4 wires from LOGO! 1 outputs (Q13 --> Q16) to LOGO! 2 inputs (I1 --> I4), you can easily have a main program in LOGO! 1 with up to 27 Digital outputs! There is even 1 spare digital output on LOGO! 2 that can be used for a remote part of the program. This idea is sCaLaBLe, so you can break the program into parts and have several LOGO!'s controlling different parts, but with some data exchange (of status's& I/O's) between them! Have fun with this - I had nothing better to do in the office today anyway! Aaaaaarrrggghh!! AttachmentUp_to_27_Outputs.zip (583 Downloads) |
This contribution was helpful to
4 thankful Users |
Follow us on