5/12/2015 5:27 PM | |
Joined: 1/4/2013 Last visit: 9/16/2024 Posts: 1124 Rating: (102) |
Dear all, I am really afraid but my TIA V13 SP1 crashes when I try to assign a variable to an I/O field in the HMI. I have one S71200 and one KTP700 and I made lot of pages with buttons/icons/IO fields, like every day. Today, after working in my PLC , I made a new page and I tried to create a new I/O field. So I browse the PLC variables and tia (wincc) freezes, and after a while pops out the crash report. I tried to close/open, reboot windows (it is Win7 Sp1) , ecc ... no way. I opened an old version of my project and the result is the same ... Omg, panic !! Attached there is the crash report, hoping that a PRO guy can help me, because it seems a very bad problem. Regards, Davinator Attachment42dbef7f-9388-4fda-bd2e-65eec2c64197.zip (110 Downloads) |
Searching for Siemens used/new equipments ? |
|
5/13/2015 7:13 AM | |
Posts: 1299 Rating: (136)
|
Hello, install the current update. https://support.industry.siemens.com/cs/ww/en/view/109311724 K!ke |
This contribution was helpful to1 thankful Users |
6/29/2015 12:59 PM | |
Posts: 1299 Rating: (136)
|
Hello, the current update is SP1 Update 3. See the link in my previous answer. K!ke |
Follow us on