3/16/2007 2:42 PM | |
Posts: 1 Rating: (0) |
Is it possible to have the hotfix for PLCSIM v5.3+SP1? |
3/18/2007 1:36 PM | |
Posts: 3149 Rating: (171)
|
Hi Hotfixes are not available via Internet, please contact Simatic Customer Support via Support Request. nemo |
6/29/2007 3:44 PM | |
Posts: 2 Rating: (0) |
I contacted to Simatic Customer Support. This is the reply (I don't know for how long it will stay available) >enclosed with this message, you receive the Link to the Hotfix 1 for >S7-PLCSIM version5.3 SP1. > > ftp://audsupport:quoo4Ueg@ftp.sbs.de/SIMATIC_S7_PLCSIM_K5.3.1.1.zip > >Please note this Hotfix is a customer- specific patch. This Hotfix is >not system- tested. > >We recommend using the next official version of this product when >available (for example the next Servicepack). |
7/26/2007 7:54 PM | |
Posts: 16 Rating: (0) |
I just made a Support Request for the Hotfix, the SFB4 TON in my simulator times out immediately also. |
7/31/2007 5:04 PM | |
Posts: 1 Rating: (0) |
Hi, |
2/18/2008 12:13 PM | |
Posts: 4 Rating: (0) |
From where did you get the Hotfix ? Can we download it from the A&D Siemens site ? Is it integrated in the SP2 of PCS7 V6.1 ? |
11/12/2008 3:02 PM | |
Posts: 16 Rating: (0) |
where TIMER_P is located, i couldn't find it. |
11/12/2008 11:25 PM | |
Posts: 2661 Rating: (279) |
CFC Library/ELEMENTA |
Follow us on