3/24/2018 7:27 PM | |
Posts: 9 Rating:
|
Hello guys! I got freezed HMI on logo indication. There is no communication to make factory reset. How can I boot from USB? Thanks! |
3/24/2018 8:21 PM | |
Joined: 10/25/2016 Last visit: 1/5/2025 Posts: 199 Rating:
|
Hi, It's possible to reload the image of the panel using "pro save", and i think you got pro save on your computer even if you never use it, this software have been installed with step7. You just need to find the CD of the image.... Otherwise take a look right Here => https://support.industry.siemens.com/cs/ww/en/view/19701610 Regards |
Last edited by: snoop13014 at: 3/24/2018 8:27:41 PMLast edited by: snoop13014 at: 3/24/2018 8:28:48 PMLast edited by: Jen_Moderator at: 3/26/2018 6:49:54 AMOptimized link. |
|
3/24/2018 8:30 PM | |
Posts: 9 Rating:
|
Hello, thanks for the reply. I 've already checked everything but I can not establish connection |
3/24/2018 8:53 PM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
|
3/24/2018 10:23 PM | |
Joined: 10/25/2016 Last visit: 1/5/2025 Posts: 199 Rating:
|
Hi, Maybe the panel adress has been lost..?? and you can't find it... Follow the link, everything is on the link, if you got the CD of panel, use it in combination with ProSave and reload the OS. Good Luck Regards Also try to check the PG/PC interface, if you try to connect to the panel using USB, check if the PG/PC Setting is correct. AttachmentProSave Picture.zip (985 Downloads) |
Last edited by: snoop13014 at: 3/24/2018 10:26:14 PM |
|
3/24/2018 10:33 PM | |
Posts: 9 Rating:
|
Hello, I don't have any cd from the panel. You mean I have to set in PG/PC s7usb and select what in the interface parameter assignment? |
3/25/2018 12:01 AM | |
Joined: 10/25/2016 Last visit: 1/5/2025 Posts: 199 Rating:
|
Hi, Parameter assignment In all case everything is describe here . If you can't load from the USB interface, it's also possible to do that using MMC and restore the panel using the MMC see=> Here Sorry if i don't answer exactly to the question but it's difficult for me because i'am not with you, and it's difficult to imagine the situation. It's midnight in my place so i gonna sleep, and i will back tomorrow in order to help you, don't worry it's not a big problem and we will find a solution to this issue, just be tenacious you got nothing to loose and if you can't repair the panel just resend it to Siemens... See you |
Last edited by: snoop13014 at: 3/25/2018 12:04:45 AM |
|
3/25/2018 11:03 AM | |
Posts: 9 Rating:
|
Hello amd thanks for the reply. I still can not establish connection.. |
3/25/2018 11:50 AM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
Hello, Please make the interface in Prosave to be Ethernet. This will enable you to make factory reset using Mac Address of the TP700. S7-USB is not suitable for factory reset of this panel based on the attached excel sheet of the following link. Which connector cables are available for connecting to SIMATIC Panels? I hope the following link will help you: |
Last edited by: Ayman Elotaify at: 3/25/2018 12:18:27 PMLast edited by: Jen_Moderator at: 3/26/2018 6:51:20 AMInserted video. Ayman Elotaify |
|
Follow us on