12/4/2012 1:41 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (713) |
Hello, Unfortunetly it's not included in Step 7 (any version), teleservice 5.1 Watch the version, should be same as your adapter. Regards, Marcjan |
Problem solved? |
|
1/28/2013 5:36 PM | |
Joined: 6/25/2009 Last visit: 2/28/2022 Posts: 11 Rating: (0) |
hi, in "Set PC/PG" interface you set communication on PC side. in "Option" - "Assign parameters TS adapter I/II" in Teleservice you set communication on PLC side and store in adapter see post /tf/WW/en/Posts/63859 best regards |
1/29/2013 2:54 PM | |
Posts: 376 Rating: (57)
|
Hello together, I still would like to give the following information. Topic: Compatibility of TeleService V6.1 SPx with the TS Adapter MPI. The TeleService software has the following compatibility of the interaction between (for example) TeleService V6.1 SP3 and a TS Adapter MPI: The version of the specific TS Adapter MPI decides the functionality, for example: - TeleService V6.1 SP3 and TS Adapter I V3.0 (achieves V3.0 functionality) -TeleService V6.1 SP3 and TS Adapter II V1.0 (achieves TS Adapter II V1.0 functionality) -TeleService V6.1 SP3 and TS Adapter I V5.2 (achieves V5.2 functionality) The operation and the configuration of the TS Adapter I V3.0 with TeleService V6.1 SP3 is therefore limited to the functionality of TS Adapter I V3.0. Note If, for example, TeleService V6.1 SP3 is used to set up the access protection in a TS Adapter I V5.x, it is no longer possible to access this TS Adapter with TeleService V3.0. Result You can use TeleService V6.1 SPx software with TS adapter V5.1. You find this information in the manual "TeleService V6.1 SP3 - Service Software for SIMATIC S7 and C7". Chapter 1, page 14. Here the link for this manual: http://support.automation.siemens.com/WW/view/en/48825184 Topic: User Rights: The following is applicable for TeleService V6.1 incl. SP5 and higher:
Best regards |
This contribution was helpful to2 thankful Users |
Follow us on