Industry Online Support
Technical Forum
8/10/2014 9:27 AM | |
Posts: 5225 Rating: (1187) |
Micheal, It would have been helpful if you said which hardware it is that you need to use. You might need to update the hardware catelog with un update. See [LINK] which links to [LINK]. Something you need to know about the files you saw in the link you provided.. You have to download ALL the files in a temporary directory. The EXE file is actually the first of an executable split archive. When you execute the EXE it will construct new files.. as if you received a ZIP file. Make sure you know where the "new" files are stored. The installation begins when you execute the unzipped install file. Having said all that.. if your PLC is of firmware 4.0, you will have a problem and will HAVE to go to TIA V13. There is however a very good chance that you have firmware V3 which TIA V11 can handle if you have made the hardware update. Does this help you? Greetings. w |
Follow us on