1/5/2018 2:03 PM | |
Joined: 9/19/2009 Last visit: 9/25/2024 Posts: 459 Rating: (85) |
Hello and Happy new year I´,m trying to upload a program from CPU 6ES7 214-1BG40-0XB0 firmware v 4.2. I have tried with TIA Portal v13 SP1, but this firmware is only avalible from TIA V14 and higher. the problem is when I tried with TIA V14 SP1 , I can´t upload because there is a warning with the version is not compatible. If I try go online , I can see version v 13, see the picture. Any help will be great Thank you |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
1/5/2018 4:35 PM | |
Joined: 9/19/2009 Last visit: 9/25/2024 Posts: 459 Rating: (85) |
Thank you very much for the tip !!! So, if with TIA V13 SP1 I can´t do it. I must install Update 1 and try, Update 2 and try etc ... and with the last update.There is 9 Updates Or Do you know if with the last update I can do it? Thank you |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
1/5/2018 4:49 PM | |
Posts: 103 Rating: (37) |
Having a lesser update installed, makes no sense to me. Update 9 for TIA V13 SP1 can be installed directly after the base installation. You should have TIA V13 SP2 if you have TIA V14. This update of V13 can be used. What I do not know: Was TIA V13 without service pack used. Hopefully that is a very slim chance. Use TIA V13 SP2 if what you have does not work. |
1/5/2018 5:09 PM | |
Joined: 9/19/2009 Last visit: 9/25/2024 Posts: 459 Rating: (85) |
I have tried with TIA Portal V13 SP1 Update 9, and I can´t go online to upload the project, however, I can see in access online, see the attachment Thank you |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
1/5/2018 6:05 PM | |
Posts: 103 Rating: (37) |
Best to play 20 questions with Siemens directly. Use the "Support Request" button that is on the web page. The support is free AFAIK. |
1/5/2018 9:30 PM | |
Joined: 9/19/2009 Last visit: 9/25/2024 Posts: 459 Rating: (85) |
Thank you for your experience |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
2/1/2018 9:01 AM | |
Joined: 9/19/2009 Last visit: 9/25/2024 Posts: 459 Rating: (85) |
Hi Yes, it is the key I have write a little guide to see how it works. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
This contribution was helpful to1 thankful Users |
Follow us on