8/14/2012 3:07 PM | |
Joined: 5/17/2007 Last visit: 9/4/2024 Posts: 39 Rating: (0) |
thank you very much TerminalBuzz, my PCS7 version is v8.0 upd1. |
8/14/2012 3:15 PM | |
Joined: 11/4/2011 Last visit: 8/25/2024 Posts: 253 Rating: (53) |
For a moment this is all I can give: MotL_to_Mot2.zip Remarks: - Mot2 type is a copy of MotL with light changes. May be useful for changing it's faceplates; - block icon type is named by the arrow direction instead of a simple number; - although every motor has it's direction arrow you would see just right arrow on the faceplate and FPs are using MotL emf files; - the number of possible trends was cutted to 6; - not used graphic objects were deleted from behind these block icons. Others are laying behind the Memo icon; - ToolTip was connected to a comment of a block, but not the tagname; - only English and Russian texts are available; - some possible states of the status bar's elements are showed; - TypeID was changed to 2012. AttachmentMotL_to_Mot2.zip (110 Downloads) |
This contribution was helpful to1 thankful Users |
8/28/2012 8:39 PM | |
Joined: 5/17/2007 Last visit: 9/4/2024 Posts: 39 Rating: (0) |
hi, i have also another question that how can i open a faceplate of a motor when i click a button? best regards |
8/29/2012 9:58 AM | |
Joined: 5/17/2007 Last visit: 9/4/2024 Posts: 39 Rating: (0) |
i need 3-4 type faceplate, for example OpDi01, OpDi03, MonDi08. |
Follow us on