5/21/2014 12:56 PM | |
Posts: 67 Rating: (1) |
Hi all, I creat new DB but i cant see Offset Column and i dont know why i cant add it as show in the PIC. Note* i have TIA V12 SP1 UPD4. |
5/21/2014 12:59 PM | |
Joined: 1/28/2009 Last visit: 4/26/2024 Posts: 6838 Rating: (1359) |
Have you read the following thread: How to see Address in Data Block.
For TIA V12, that is available in properties of a DB(Right click on DB-->Properties-->attribute--> Optimied block access. But before un-check read the following: STEP 7 Professional V12.0 (01/2013, English) wrote: ProcedureTo set the block access, proceed as follows:
|
Last edited by: hdhosseini at: 5/21/2014 1:06 PMLast edited by: hdhosseini at: 5/21/2014 1:01 PM |
|
This contribution was helpful to3 thankful Users |
5/21/2014 1:04 PM | |
Posts: 67 Rating: (1) |
Thanks bro :$ i will read thanks a lot |
5/21/2014 1:07 PM | |
Joined: 3/24/2009 Last visit: 6/20/2023 Posts: 535 Rating: (112) |
Dear AZRAIQI, if you have created your DB with the option "Standard - compatible with S7-300/400" (if available), you will see the offset-column. If you didn't set this option, or if the option is not available for this CPU, you only can access your DB-elements symbolic. Have a look at this link. Best regards, yy1 |
Last edited by: yy1 at: 5/21/2014 1:08 PMtoo slow Hamid was faster and better |
|
5/21/2014 1:15 PM | |
Joined: 3/24/2009 Last visit: 6/20/2023 Posts: 535 Rating: (112) |
Dear AZRAIQI, you can change this in the block-attributes -> Optimized block access Best regards, yy1 |
Last edited by: yy1 at: 5/21/2014 1:15 PM |
|
This contribution was helpful to1 thankful Users |
5/21/2014 1:17 PM | |
Posts: 67 Rating: (1) |
Thanks man, i follow your link and by default in my program it "Optimized Block Access"and still i cant see the address
|
Last edited by: AZRAIQI at: 5/21/2014 1:23 PM |
|
5/21/2014 1:28 PM | |
Posts: 67 Rating: (1) |
So why i get an error when i compile the program see that and |
Follow us on