6/29/2006 2:22 PM | |
Posts: 13 Rating: (0) |
Hello [:D], My question is this: - How can l read the database of WinCC v6.0.3 in the Microsoft Office - Excel, into the PC Server? Thanks Vítor |
6/29/2006 3:34 PM | |
Posts: 3149 Rating: (171)
|
Hi, this issue has already been discussed several times here in this forum, so just search for "wincc excel" /tf/WW/en/Posts/1487 nemo |
6/30/2006 12:43 PM | |
Posts: 13 Rating: (0) |
Hi, sorry, but i had another question: - Can i access to the WinCC v6.0database in a PC with WinCC installed, without license, with dat@monitor. What do you recommends (i have to analysis WinCC database): - Datamonitor or Connectivity Pack? Thanks, Vitor |
6/30/2006 1:06 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (150)
|
[quote user="Vitor"] - Can i access to the WinCC v6.0database in a PC with WinCC installed, without license, with dat@monitor. Technically yes as WinCC runs in demo mode. However you would be in breach of your licensing agreement. Is this what you meant? [quote user="Vitor"] What do you recommends (i have to analysis WinCC database): - Datamonitor or Connectivity Pack? If you are familiar with databases, SQL and programming then use the Connectivity Pack. If you are not familiar then use DataMonitor If the end-user wants to build their own reports or do ad-hoc analysis then you should use DataMonitor. DataMonitor involves NO programming and is designed to be used by end-users Connectivity Pack is a developers tool and designed to be used by developers / systemintegrators. Basically it all comes down to your / your customer's expectations and skill set. |
7/5/2006 10:57 AM | |
Posts: 13 Rating: (0) |
Vitor wrote: - Can i access to the WinCC v6.0database in a PC with WinCC installed, without license, with dat@monitor. Technically yes as WinCC runs in demo mode. However you would be in breach of your licensing agreement. Is this what you meant? ------------------------------------------------------------------------------------------------------------------------------- What license do i need to buy to not breach thelicensing agreement, in this case? |
7/6/2006 9:38 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (150)
|
You would need a DataMonitor licence [:)] Further info at http://support.automation.siemens.com/WW/view/en/22449045 |
8/9/2006 9:18 PM | |
Posts: 1275 Rating: (123) |
It's kinda comforting to know that I'm not the only one who stumbles into unpredictable unexplained problems with these softwares from time to time! [:D] |
Follow us on