12/2/2016 1:29 PM | |
Joined: 6/24/2013 Last visit: 3/1/2021 Posts: 1444 Rating:
|
Hi 1. set the telegram in the drive --> drive manual + any CD etc. 2. download GSD for the drive so you can configure it 3. use SFC (14 and 15 if I remember correct - DP Write and Read) to get the data to/from drive 4. data is written to/from local temp variables organized as per the telegram. I have function for Siemens Micromaster and I did not bother with SFC because it was couple of words - used load/transfer to do copying. the code can be used as a sketch but your process data will be different --> Yaksawa manual. Attached: Printout of comms block. Attachment!MM440_Comms_printout.pdf (16 Downloads) |
Follow us on