1/25/2022 12:03 PM | |
Joined: 6/3/2013 Last visit: 5/23/2025 Posts: 50 Rating:
|
Hi, One of these examples will help you: |
And you will know the truth, and the truth will set you free. |
|
1/25/2022 3:14 PM | |
Joined: 3/27/2008 Last visit: 9/14/2025 Posts: 1216 Rating:
|
I have attached a file for setting the V20 for PI control, P304 to P1910, then selecting PI control for Macro Cn009. The settings for fixed frequency setpoint can be change for an analogue, id Fixed Frequency is not suitable. Parameter P704 is set to 99, this makes digital Input 4, available for selecting Manual or PI control. P2200, enables the PI controller, this is set to look at Digital Input 4 for a 'high', this 'high' enables the PI control. Also, see the 'notes' for useful PI settings to get the thing working. Hope this works for you, come back if we can help further. Tractor AttachmentV20 PI.pdf (757 Downloads) |
Tractor |
|
Follow us on