6/22/2009 7:11 PM | |
Joined: 9/27/2006 Last visit: 8/21/2025 Posts: 47 Rating:
|
Hi All, I just installed a CAS 7.0 and the data isn't getting processed correctly by the server. I'm using in the WinCC Server 1 Day per segment / 1 week for all segments, and in the CAS 1 Day per segment and 1 Year for all segments. The database files seems to be copied correctly to the ArchiveDir folder, but Igetan error message "Archive Failed" in the Application Log screen. (See attached picture). Has anyone seen this problem before? Can I find some better informationabout this error? Thanks! AttachmentCAS_Config.zip (561 Downloads) |
6/22/2009 8:17 PM | |
Joined: 9/27/2006 Last visit: 8/21/2025 Posts: 47 Rating:
|
Hi rit03, thanks for your reply. I'm not sure if I understood what you suggested. So far, I configured the WinCC Server to backup the files in the CAS Server (over the Network). This step seems to be fine, as I can see multiple files in the ArchiveDir folder. After these files are copied, I see in the Aplication Log the info "Start Processing". I'm not sure what the CAS is doing in this step, but after few minutes it renames the extension of all files to ".failed" and the info comes as "Archive Failed". I don't knowwhere it is failing... (See the attached pictures). Are you suggesting that I change the Backup path to the local drive in the WinCC Server? What should I watch out then? The CAS Application is running only in the CAS Server, right? Thanks! AttachmentCAS_ArchiveDir.zip (471 Downloads) |
6/22/2009 11:21 PM | |
Joined: 6/13/2006 Last visit: 2/11/2023 Posts: 341 Rating:
|
Please find the attached guidline to setup back-up archive for CAS and check you have done all the necessary settings. regards, rit03 AttachmentBackup_CAS.pdf (733 Downloads) |
9/22/2009 8:26 AM | |
Posts: 2 Rating:
|
Hi, Did the re-install fix this? Im curious as I have very similar issue. Thanks. |
Follow us on