2/9/2011 1:20 PM | |
Joined: 12/12/2005 Last visit: 3/17/2024 Posts: 180 Rating:
|
Hi, Maybe you have some ideas... My problem´s are Masterdrive MC´s 6ES7013(15 and18)-0EP50-Z, Z=C23+G91+F01. We have CPU315-2DP and 3xMasterdrives in Profibus DP 12Mpbs. Ineed to upload Masterdrive parameters and see diagnostic and faults and alarms. I downloaded DriveMonitor from: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=11769381&caller=viewprogram working it´s fine. Problem is to connect online to Masterdrives. 1. I try by profibus connect RS485 to top of busconnector6es7972-0BB11-0XA0. CPU´s BF and SFgoing faultwhen I putconnector on. I have right speed and etc. Bus is connected CBP2 card. 2. Then I connect RS485 to X103 no connection. 3. Then I made special RS232 cabel and try online by X103, not working? So if someone have good Idea where I go wrong, please answer. Manual: mc24_kompend_e[1].pdf link: http://www2.ad.siemens.com.cn/download/Upload/MC/manual/MC%20V2.4.pdf?bcsi_scan_84C833B65C0B3F5A=1 Regards -Heksu- Splitted from Programming programs general. |
Last edited by: Heksu at: 2/9/2011 2:36 PMManual link Last edited by: O_Moderator at: 2/9/2011 1:51 PMnew subject after splitting "Beer is proof that God loves us and wants us to be Happy"-Benjamin Franklin |
|
2/9/2011 1:59 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Using DriveMonitor is possible to connect to the drive using serial cable. The pins is available at mentioned manual (on 108th page). So, you need serial port on PC. Be careful when using USB to Serial convertors. Look at My PG/PC has only USB com-ports. How I can get online with my drive? Best regards, Hristo Mihalev |
2/10/2011 5:22 AM | |
Posts: 27 Rating:
|
Dear Heksu, Please go through attached file Attachmentmasterdrive upload .pdf (2411 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on